No. 1 global supplier of Machine Safety Source: ARC Advisory Group

Share this page  
The planned merger of (EN) ISO 13849 and IEC 62061 stopped

The planned merger of (EN) ISO 13849 and IEC 62061 stopped

Until very recently it was intended that a new safety standard IEC/ISO 17305 would merge (EN) ISO 13849 and IEC 62061. IEC/ISO 17305 was expected to take effect in 2017, giving users a single global safety standard, and clarifying some of the issues encountered while trying to comply with two similar but separate standards. However, the IEC/ISO 17305 project was stopped.

Read more
What's new in safety legislation

What's new in safety legislation

Watch this video and find out for yourself.

Watch video
(EN) ISO 14119 – Interlocking devices associated with guards

(EN) ISO 14119 – Interlocking devices associated with guards

The international standard which provides guidance on the design and selection of safety interlocking devices has been significantly revised.

Watch video